The following table lists the types of graphics you can associate with the types of objects. In
SCT, you can associate graphics to a space object, equipment object, and field
controller.
| Object type | Standard Graphic using SCT | Graphics+ Graphic using SCT |
|---|---|---|
| Space object | Yes | Yes |
| Equipment object | Yes | Yes |
| Field controller | Yes | Yes |
You can associate multiple graphics of the same type or of varying types to each object or field controller. If an object has multiple graphics associated with it, a count of the number of the graphics appears in the Graphics widget.
Note: Do not place graphics in the
Facility Graphics folder or folders nested within it in the All Items tree. Graphics
saved in this folder are Metasys UI graphics saved by the system that you should not
edit in SCT. Equipment and graphics are not viewable in SMP, therefore, the Facility
Graphics folder is not displayed in SMP.
Figure 1. Facility graphics folders

At Metasys UI Release 2.1 and later, graphics associations can be managed in the Graphics Manager of the Metasys UI and Metasys UI Offline. For more information, refer to the Metasys UI Help (LIT-12011953) , Metasys UI Custom Symbols Technical Bulletin (LIT-12013054) , or Metasys UI Offline Help (LIT-12012116) .