Adding the Metasys UI site as a bookmark in Launcher - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

About this task

To add the Metasys UI as a bookmark profile:

Procedure

  1. Open the Launcher.
  2. On the Launcher screen, click Add, then click the Bookmark tab. The Add New Screen appears.
  3. Type a description for the profile. For example, you could specify My Metasys UI in this field.
  4. Type the URL for the profile. For example, https://localhost/UI if you are creating the bookmark on the ADS/ADX/OAS or ADS-Lite computer. Or, https://[hostname]/UI, where [host name] is the host name, server name, or IP Address of the ADS/ADX/OAS or ADS-Lite computer. Use the fully qualified computer name to avoid the certificate warning pop-up screen.
  5. Select Create Shortcut to create a shortcut icon on your desktop.
  6. Click Save. The new profile is saved, and the Launcher main screen appears with the new profile shown under the Bookmark tab. If you clicked Create Shortcut, a shortcut labeled with the Description you entered is created on the computer desktop.