About this task
To add the Metasys UI Offline as a bookmark profile:
Procedure
- Open the Launcher.
- On the Launcher screen, click Add, then click the Bookmark tab. The Add New Screen appears.
- Type a description for the profile. For example, you could specify My Metasys UI Offline in this field.
- Type the URL for the profile. For example, https://localhost/UIOffline if you are creating the bookmark on the SCT computer. Or, https://[host name]/UIOffline, where [host name] is the host name, server name, or IP Address of the SCT computer. Use the fully qualified computer name to avoid the certificate warning pop-up screen.
- Select Create Shortcut to create a shortcut icon on your desktop.
- Click Save. The new profile is saved, and the Launcher main screen appears with the new profile shown under the Bookmark tab. If you clicked Create Shortcut, a shortcut labeled with the Description you entered is created on the computer desktop.