Optimize the required storage size of the ADS/ADX /OAS Trend repository using the following methods:
-
configure larger sample intervals for individual trends
-
determine which trends to store long-term and transfer only these samples
-
configure the trends of non-critical objects to sample on large Change-of-Value (COV) increments
In addition, optimize the network communication performance for transferring trend samples from network engine devices to the ADS/ADX /OAS repository using the following methods:
-
configure the Transfer Setpoint on individual trends so they transfer their samples at intervals different from other trends
-
use the ADS Delivery Time of the network engine device to transfer the samples at the time when user access to the system is minimal
Refer to the Trend extensions topic in the Metasys UI Help (LIT-12011953) for more information.