The following table lists the corresponding features of the Metasys UI that use the repository databases.
|
Repository |
Metasys UI feature |
Database |
|---|---|---|
|
Trends |
Reporting data that displays in the Trend widget and the Custom Trend viewer; syncs with the JCIReportingDB repository at installation and then once in every 24-hour period |
JCIHistorianDB |
|
Audits |
Audit data for user and system commands and user annotations on commands that display in the Equipment Activity widget and System Activity. |
JCIAuditTrails |
|
Events |
Alarm data, event message annotations, and user annotations on alarm events that display in the Equipment Activity widget, Alarm Panel, Alarm Manager, and Alarm Monitor |
JCIEvents |
|
Reporting |
Reporting data that displays in the Trend widget and Custom Trend viewer |
JCIReportingDB |
|
Spaces Authorization |
User permissions data for Spaces and Custom Dashboard settings |
SpacesAuthorization |
|
Potential Problem Areas |
Point data that displays in the Points tab of the Potential Problem Areas widget. The database self-maintains and stores a rolling seven days' worth of data. |
MetasysValue Note: You need to license the Potential Problem
Areas Points on an OAS to activate the MetasysValue
database.
|
|
Fault Detection |
Fault data that displays in the Faults tab of the Potential Problem Areas widget. The database self-maintains and stores a rolling seven days' worth of data. |
MetasysFault
Note: You need to license the Fault Detection
feature to activate the MetasysFault
database.
|
|
Fault Triage |
Fault Triage data that displays in the Fault Triage feature. |
MetasysFaultTriage
Note: You need to license the Fault Triage
feature to activate the MetasysFaultTriage
database.
|
At installation time, the JCIHistorianDB synchronizes with the JCIReportingDB. This initial synchronization can take several hours. The average synchronization takes an hour per 5 to 10 GB. While the synchronization takes place, the Metasys UI Trend widget is available, but the historical trend data may not appear until the synchronization is complete.
The Metasys UI does not support annotations on objects, such as an engine, controller, or points.