Audit repository optimization - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

Optimize the required storage size of the ADS/ADX /OAS Audit repository by specifying the Audit level (1 through 4) for the audit messages that need to be reported and archived.

In addition, optimize the network communication performance for transferring audit messages from network engine devices to the ADS/ADX /OAS Event repository by optimizing the Audit repository size in the device object of each network engine.

Audit Level 1 provides the minimum information. Audit Level 4 provides the most information. Audit Level 2 is the default setting. Refer to the Audit Trail topic in the Metasys SMP Help (LIT-1201793) for more information.