A repository provides long-term storage for historical data. Typically, the Server configured as the Site Director also provides the individual repositories for trend data, event messages, audit messages, annotations, reporting, and spaces authorization data. Individual repositories may reside in the SQL Server database. For a split ADX, the repositories are on the database server where the SQL Server software is installed. You can install a split ADX where the database server computer stores all historical data. On an OAS, the amount of historical data retained in its repositories (and therefore available to Metasys UI) is affected by the Metasys Historical Data Add-on license.
The following table lists the ADS/ADX/OAS repositories, the corresponding online Metasys SMP Help (LIT-1201793) or Metasys UI Help (LIT-12011953) topic, and the corresponding file name. The next sections describe the repositories in more detail and suggest ways to optimize the repositories.
Repository |
Refer to |
Database file name on the ADS/ADX /OAS computer |
---|---|---|
Trends |
Trend extensions in the Metasys UI Help (LIT-12011953) |
JCIHistorianDB |
Audits |
Audit Trail in the Metasys SMP Help (LIT-1201793) |
JCIAuditTrails |
Events |
Alarm and Event Management in the Metasys SMP Help (LIT-1201793) |
JCIEvents |
Annotation
Note: Metasys UI does not use this
database.
|
Object Message Annotations in the Metasys SMP Help (LIT-1201793) |
JCIItemAnnotation |
Reporting |
Advanced Reporting in the Metasys SMP Help (LIT-1201793) |
MetasysReporting |
Metasys UI Reporting |
Reporting: Trend Widget and Custom Trend Viewer in the Metasys UI Help (LIT-12011953) |
JCIReportingDB |
Spaces Authorization |
Space Authorization and Dashboard Manager in the Metasys UI Help (LIT-12011953). |
SpacesAuthorization |