Installing the Metasys UI - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

The Metasys UI is installed as part of Metasys Server installation. For more information about installing the Metasys Server and the Metasys UI, refer to the Metasys Server Installation and Upgrade Instructions Wizard (LIT-12012162) or the Metasys Server Lite Installation and Upgrade Instructions (LIT-12012258).