Security certificate warnings - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active
When browsing to the Metasys UI Offline, if the Metasys UI Offline site does not have a trusted security certificate, the web browser displays a security certificate warning.
Note: Metasys UI uses cookies as part of its protocols, so ensure that your web browser does not block all cookies before you browse to the Metasys UI Offline.
If you see this warning, browse to the Metasys UI Offline site by doing the following:
  • For Google® Chrome™:
    1. Tap or click Advanced.
    2. Tap or click Proceed to [IP Address], where [IP Address] is the IP Address of the SCT computer. The Metasys UI Offline login screen appears.
  • For Microsoft Edge: Tap or click Continue to this website (not recommended). The Metasys UI Offline login screen appears.
  • For Apple® Safari® 11 or later: Tap or click Continue in the Cannot Verify Server Identity window. The Metasys UI Offline login screen appears.
Note: The Metasys UI Offline does not support auto-complete functionality for the user name or password fields.

We strongly recommend installing a trusted security certificate. For more information about security certificate implementation for the Metasys UI Offline, see refer to the SCT Installation and Upgrade Instructions (LIT-12012067).