Browsing to the Metasys UI Offline - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

To browse to the Metasys UI Offline from a client computer or device, in a supported web browser go to https://[host name]/UIOffline, where [host name] is the host name, server name, or IP address of the SCT computer.

To access the Alarm Monitor, you do not need to log in to your Metasys UI site. Simply navigate to https://[host name]/UI/alarms, where [host name] is replaced with host name, server name, or IP address of your Metasys Site Director. However, an administrator user must first log in to the Metasys UI Online and enable the Alarm Monitor after you install the Metasys UI.