Data usage - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

When you first navigate to the Metasys UI, the Metasys UI consumes approximately 3.8 MB of bandwidth. The following table shows typical data consumption for one user on a site.

Table 1. Metasys UI bandwidth consumption
Initial page navigation once logged into the Metasys UI: 3.8 MB
Subsequent page navigation after the Metasys UI is cached:

Space dashboard

Approximately 275 KB

Equipment dashboard

Approximately 326 KB

Per minute data consumption

Approximately 30–200 KB