Space Authorization in the Metasys UI - Metasys - LIT-12012115 - Server - Metasys UI - 11.0

Metasys UI Technical Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
Technical Bulletin
Document number
LIT-12012115
Version
11.0
Revision date
2020-10-30
Product status
Active

Metasys system administrators can set user authorization for spaces in the Metasys UI. The space authorization is not the same authorization or permissions granted in the Site Management Portal (SMP) or in the SCT. The space authorization set in the Metasys UI is not available in the Metasys UI Offline, and does not affect the Metasys UI Offline.

Metasys system administrators can set space authorization for other users by selecting the Space Authorization option in the User Menu in the Metasys UI (Administrative Tasks). The following table describes the three authorization options available per space.

Table 1. Space Authorization options

Option

Description

Allow

Allow access to the space dashboard, the equipment dashboard of the equipment directly serving the space, and any associated alarms, schedules, and graphics for the space.

Deny

Deny access to the space dashboard, the equipment dashboard of the equipment directly serving the space, and any associated alarms, schedules, and graphics for the space.

Inherit

Inherit authorization from the parent space.

Space authorization information is contained in the Spaces Authorization database.

For more information about space authorization, refer to the Space Authorization section in Metasys UI Help (LIT-12011953) .