Working with the Tools Tab - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

How do I use the Import Custom Symbols option?

To use the Import Custom Symbols option, click IMPORT CUSTOM SYMBOLS. For more detailed information about the Import Custom Symbols option, see Working with Symbols.

How do I use the Export Custom Symbols option?

To use the Export Custom Symbols option, click EXPORT CUSTOM SYMBOLS. For more detailed information about the Export Custom Symbols option, see Working with Symbols.