Working with the Graphics List - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

What do the icons in the Graphics List represent?

The following table describes the icons that feature in the Graphics List.
Table 1. Graphics List icons
Icon Icon name Icon description
Add new graphic Creates a new graphic.
Copy Copies a Metasys UI graphic.
Paste Pastes the Metasys UI graphic you copied.
Sort down Moves the graphic down in the list.
Sort up Moves the graphic up in the list.
Delete Deletes the graphic from the list.
Aliased graphic enabled This icon displays, when Aliased graphics are enabled. This applies to the Graphics List for a piece of equipment and for an Equipment Definition.
Aliased graphic disabled This icon displays, when Aliased graphics are disabled. This applies to the Graphics List for a piece of equipment and for an Equipment Definition.