Creating Equipment, Space, Network, or Unassigned Graphics - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

What is a network graphic?

A network graphic is a Metasys UI graphic associated with a network object.

How do I create a network graphic?

  1. Select the Graphics tab.
  2. Select Network from the list and select a network object.
  3. Click + or +ADD GRAPHIC in the Graphics List. The New Graphic window opens.
  4. Select a template from the Default list or the Custom list.
  5. Enter a name in the Name field.
    Note: The following are invalid characters for a graphic name: <, >, :, ", /, \, ?, *, |, @, #, . (period), and , (comma).
  6. If required, enter a description.
  7. Select an authorization category.
  8. Click CREATE. The graphic opens in the Graphic Editor. For more information on working with the Graphics Editor, see Graphics Editor.