How do I modify a trend study in the Network tree? - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

Procedure

To modify a trend study that you created in the Network tree, complete the following steps:

  1. In the Network tree, select a trend study.
  2. To add points to a trend study, complete the following steps:
    1. In the Trend Study widget, click the Change Points icon.
    2. Click ADD POINTS or CHANGE POINTS. The button that displays depends on if points have already been added or not.
    3. In the Add & Remove Points window, from the drop-down list, select a location.
    4. From the tree or list that displays, locate and select the points (trends) that you require. You can add a maximum of 32 points to a trend study.
    5. To add the points to the trend study, click the Right Arrow icon.
    6. Click SAVE.
  3. To change the points that are visible on a trend study, complete the following steps:
    1. From the points list, select the check boxes of the points that you want to display on the trend study. You can select up to 10 points.
    2. Click APPLY.
  4. To remove points from a Trend study when you are logged on to Metasys UI on a server, use the Trend Study Manager as outlined in How do I edit a trend study in the Trend Study Manager?
  5. To remove points from a Trend study when you are logged on to Metasys UI on an engine, complete the following steps:
    1. In the Trend Study widget, click the Change Points icon.
    2. Click CHANGE POINTS.
    3. In the Selected pane, select the points that you want to remove.
    4. Click the Left Arrow.
    5. Click SAVE.
  6. To quickly remove all of the points from the trend study, complete the following steps:
    1. In the Trend Study widget, click the Change Points icon.
    2. Next to the CHANGE POINTS button, click the Clear All link.
    3. Click CLEAR ALL.