How do I delete a trend study in the Network tree? - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

Procedure

To delete a trend study in the Network tree, complete the following steps:

  1. In the Network tree, select a trend study.
  2. In the Create and Delete Object toolbar for the Network tree, click the Delete icon.
  3. In the confirmation window, click DELETE.