How do I create a trend study in the Network tree? - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

Procedure

You can create trend studies from the Network tree and use the Trend Study widget to view and edit the trend studies. To create a trend study in the Network tree, complete the following steps:

  1. In the Network tree, select the location where you want to create the trend study.
  2. In the upper left of the Network tree, click the + icon. The Create Item wizard opens.
  3. In the Create Item window, complete the following steps:
    1. From the General Type list, select Object.
    2. From the Object Type list, select Trend Study.
    3. In the Unique Identifier field, review the unique identifier, and change it if required.
    4. Click NEXT.
    5. Configure the trend study as required, and click CREATE. The trendy study appears in the network tree and its Network dashboard displays the Trend Study widget.