Custom Trend - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

What is a live point and how do I add it to Custom Trend?

A live point is a point that does not have a trend extension on its default value. When you add a live point, Custom Trend displays a live trend of the point's default value, for example Present Value. A live trend gets plotted from the current time until the session finishes or the point is removed from Custom Trend. You can add a live point to Custom Trend in the same way as you add trend series.

How do I switch from a line graph to a bar graph? How do I switch to a candlestick graph?

How can I create a Trend Study in Custom Trend?

  1. In Custom Trend, click or tap the Change Points icon (pencil) in the upper right of the screen.
  2. Click or tap CREATE TREND STUDY.
  3. Click or tap APPLY.