Equipment Trend widget, Building Network Trend widget, Custom Trend viewer, Trend Study widget, and Trend Study Manager - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

Can I view raw and aggregated data for all time ranges?

Yes, starting at Metasys Release 11.0, you can view either raw or aggregated data in a trend chart for all different time ranges. The default selection is Raw Data mode. Use the Settings icon to switch between Raw Data and Aggregate Data.
Note: Aggregation is not supported for trend studies that are located on engines.

Can I view historical data for a disabled trend extension?

You can view historical data present for a point on all trend widgets and on the Custom Trend viewer, based on the time range you select. A triangle icon indicates a disabled trend extension.