What is the Equipment Relationships widget?
Use this widget to see all relationships a piece of equipment has with other equipment, spaces, and network field controllers. You can easily navigate to other equipment or spaces to help troubleshoot issues.
What is the layout of the Equipment Relationships widget?
The following figure and table describe the layout of the Equipment Relationships
widget.
Figure 1. Equipment Relationships widget callouts

Number |
Name |
Description |
---|---|---|
1 | Network Area | Displays the online or offline status of all the network controllers that manage the piece of equipment. |
2 | Served By Area | Shows all of the equipment that the piece of equipment is directly served by. |
3 | Serves Equipment Area | Shows all of the equipment that the piece of equipment directly serves. |
4 | More Button | Shows the remaining data. |
5 | Serves Spaces Area | Shows all of the spaces that the piece of equipment directly serves. |
What information appears in the Equipment Relationships widget?
The Equipment Relationships widget displays:
- The network controllers the points are located on, including their online or offline status information
- The equipment that directly serves the piece of equipment (if any)
- The equipment that is directly served by the piece of equipment (if any)
- The spaces that are directly served by the piece of equipment
What information appears in the Equipment Relationships widget for a Building Network tree object?
The Equipment Relationships widget includes the spaces, equipment serving the spaces, and the
equipment that serves other equipment in a serving-relationship tree. You can tap or
click on the space or equipment to go to that space or equipment's dashboard.
Figure 2. Equipment Relationships widget for Building Network object

How do I view all of the controllers, equipment, or spaces that are related to a piece of equipment?
If there are more controllers, equipment, or spaces to view, tap or click > MORE to view all of them. If there are no other controllers, equipment, or spaces to view, > MORE does not appear. To see fewer controllers, equipment, or spaces, tap or click LESS.
Is the Equipment Relationships widget supported on all devices?
Yes, the Equipment Relationships widget is supported on desktop, tablets, and smartphones.