The following table lists the icons that appear on the home screen of the Metasys UI .
| Icon | Icon name | Icon description |
|---|---|---|
|
|
Hamburger | Opens or closes the navigation panel, which includes the Spaces tree and the Building Network tree. |
|
|
Search | Opens a field to search for spaces and equipment. Appears only when logged in to the Site Director for a site that supports spaces and equipment. For more information, see What Metasys sites support spaces and equipment?. |
|
|
Custom Trend | Opens the Custom Trend viewer. |
|
|
Alarm |
Opens the Alarms list. Appears on smartphones when you are
using Metasys UI for a Metasys server on a non-MVE site. See
Alarms on smartphones (Alarms list) for details.
Note: Before Metasys Release
12.0.50, this icon also appears for desktop and tablet with the
other listed icons and opens Alarm Manager. From Metasys Release
12.0.50, a similar icon appears in the Alarm Notification Bar
for desktop and tablet when applicable. See Alarm Notification Bar for details.
|
|
|
System Activity |
Opens System Activity.
Appears on smartphones when you are using Metasys UI for an
engine or an MVE site. See System Activity for
details.
Note: For
desktop and tablet, a similar icon appears in the Alarm
Notification Bar when applicable. See Alarm Notification Bar for details.
|
|
|
User menu | Opens user menu options. |
The explanation for the icons related to widgets and specific features is in the section where the widget or feature is described.