Overview - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

How do I access Metasys UI Help on engines?

The User menu in the Metasys UI provides an option to open the Metasys UI Help. For servers, this opens the Metasys UI Help file that is stored on the server. For engines, this opens the Metasys UI Help file that is published to the Internet because the Help file is not stored on the engine itself.

If you are logged on to Metasys UI on an engine, and your browser is not connected to the Internet, the Metasys UI Help cannot load from the User menu. In this case, use a browser on a different device that is connected to the Internet, and navigate to the following address: https://docs.jci.com/JohnsonControls/Metasys-UI-Help