Runtime totalization - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The Runtime totalization extension tracks the time that elapses while a designated input, such as a binary or multistate value, matches a specified state.

These two essential parameters determine the Runtime totalization extension’s mode of operation:

  • the monitored Input Reference
  • the Reference (state) that identifies active runtime

Use this extension to track the amount of time that a piece of equipment, such as a fan or a pump, is operational. This extension also determines the amount of time that a point is in alarm or the runtime of fixed loads (such as lighting) for energy consumption and tenant billing.

The Runtime totalization extension contains attributes common to Metasys system objects. The following table lists the attributes specific to the Runtime totalization extension.

Note: In the Notes column, the letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
Table 1. Runtime totalization attributes

Attribute name

Notes

Initial value

Values/Options/Range

Description

Display Precision

C,W

10ths

Uses Display Precision (Set 0).

Executing

 

Active

Active

Totalize Limit

Inactive

Active: The extension is calculating and has not reached the Totalize Limit.

Totalize Limit: The extension has reached the limit and has stopped calculating because Rollover is set to False.

Inactive: The extension is unreliable or disabled and is not calculating.

Input Reference

C

   

Present Value

C,D,R,W

   

Reference

C,W

State 1

States Test attribute identifies the enumeration set for this attribute.

Reliability

 

Reliable

Uses Reliability (Set 503).

Reset

(This attribute does not appear in a view, but may be scheduled, trended, and so on.)

W

False

False

True

Reset Date

     

Reset Time

     

Rollover

C,W

False

False

True

Rollover Count

R,W

0

0–4,294,967,295

States Text

(This attribute does not appear in a view, but may be scheduled, trended, and so on.)

C,W

States

 

Timebase

C,W

Hours

Seconds, minutes, hours, days

Totalize Limit

C,N,W

Hours

 

Units

C,W

No Units

 

Value Before Reset