Event totalization - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The Event totalization extension tracks the number of binary events or pulses over time, meaning it counts the number of transitions that occur at an input reference. Unlike other types of totalization, event totalization increases the value each time the event occurs, instead of calculating the value once each minute.

These three essential parameters determine the mode of operation for the Event totalization extension:

  • the monitored Input Reference
  • the types of recorded Transitions or events
  • the recorded Value Per Pulse (event)

You can use this extension to determine the number of changes in an input value, which may be helpful for maintaining and monitoring equipment. For example, use Event Totalization to determine how many times a motor started, how often a sensor was in alarm, or how many cars entered a parking lot.

The Event totalization extension contains attributes common to Metasys system objects. The following table lists the attributes specific to the Event totalization extension.
Note: The letters in the Notes column indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
Table 1. Event totalization attributes

Attribute name

Notes

Initial value

Values/Options/Range

Description

Display Precision

C,W

1s

Uses Display Precision (Set 0).

Executing

 

Active

Active

Totalize Limit

Inactive

Active: The extension is calculating and has not reached the Totalize Limit.

Totalize Limit: The extension has reached the limit and has stopped calculating because Rollover is set to False.

Inactive: The extension is unreliable or disabled and is not calculating.

Input Reference

C

   

Present Value

C,D,R,W

   

Reference

C,W

State 0

States Text attribute identifies the enumeration set for this attribute.

Reliability

 

Reliable

Uses Reliability (Set 503).

Reset

(This attribute does not appear in a view, but may be scheduled and trended.)

W

False

False

True

Reset Date

     

Reset Time

     

Rollover

C,W

False

False

True

Rollover Count

R,W

0

0–4,294,967,295

Scale Factor

C,W

1.0

Minimum Value > 0

States Text

(This attribute does not appear in a view, but may be scheduled and trended.)

C,W

States

 

Totalize Limit

C,N,W

   

Transition

C,W

Entering State

Entering State

Count All

Units

C,W

 

IP

SI

Value Before Reset

     

Value Per Pulse

C,W

1