Normal state - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

Normal state occurs when the alarm extension is in an acceptable, expected condition, as indicated by the attribute point to which it is added.