Multistate alarm extension - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The multistate alarm extension adds the alarming capability for an attribute with True or False, or Multistate data types, such as the Present Value of a Binary Input Object.

The multistate alarm extension detects the alarm with respect to a difference from a defined normal state and sets the Alarm State attribute of the object to which it is added. In addition, you can configure the multistate alarm extension to report alarms and True or False and/or Multistate events.