Multistate alarm attributes - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The multistate alarm extension contains attributes common to Metasys system objects.

The following table lists the attributes specific to the multistate alarm extension.

Note: In the Notes column, letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable. Attributes marked with a C are editable while you are creating the object, and attributes marked with a W are editable after the object is created..
Table 1. Multistate Alarm Attributes

Attribute name

Notes

Initial Value

Values/Options/Range

Description

Alarm Ack Pending

 

False

Ack not pending, Ack pending

Alarm Ack Required

C,W

False

Ack not required, Ack required

Alarm Date

     

Alarm Message Text

C,N,W

   

Alarm Priority

C,W

70

Alarm Time

     

Alarm Values

C,W

   

Capture Changes

 

False

 

Command Reference

C,W

   

For more information on how this attribute works with regard to AO/BO point feedback, see AO/BO Feedback.

Date

     

Indicates the date of the last reported condition.

Event Enable

C,W

True

 

Graphic

C,N,W

Null

Object Type = Graphic

Graphic Alias

C,W

 

Maximum 256 characters

Input

   

Derived from Input Reference, the object to which the Multistate Alarm extension has been attached.

Input Reference

C

   

Normal Ack Pending

 

False

Ack not pending, Ack pending

Normal Ack Required

C,W

False

Ack not required, Ack required

Normal Date

     

Normal Priority

C,W

200

Normal Time

     

Normal State

C,W

State 0

Derived from Input Reference, the object to which the Multistate Alarm extension has been attached.

Present Value

D,R

Normal

Normal, Alarm, Hold

Reference Delay Time

C,W

0

0–65,535 seconds

When a Binary Output Object (BO) (supply fan command) is commanded On, the Normal State for the associated Binary Input Object (BI) (supply fan status) alarm extension is also On. After the Reference Delay Time, the current state of the BI is compared to the Normal State. If the BI is still Off, an alarm is detected. The Reference Delay Time is also used when the BO is commanded Off.

Specifies the feedback delay in seconds. The purpose of the Reference Delay Time is to allow time for equipment to start or stop before the status is compared to the command.

Reference Delay Timer Active

 

False

 

Reliability

 

Input Unreliable

Uses Reliability (Set 503).

Report Delay

C,W

0

0–65,535 seconds

Report Delay Active

C,W

False

 

Status

     

Disabled: Enabled attribute value is False.

Unreliable: Reliability attribute is not reliable.

Normal: Expected operating condition.

Time