Schedule widget for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The Schedule widget for MVE on Metasys UI functions in the same manner as for a non-MVE site, with the following differences.

If the schedule requires an MVE annotation or MVE electronic signature and you modify the schedule in any way, you are prompted for MVE validation when you save the changes. This applies to any changes you make to the schedule within its Schedule widget, including changes to its Weekly Schedule, Exceptions, Scheduled Items, or Details.