Schedule summary widget for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The Schedule summary widget for MVE on Metasys UI functions in the same manner as for a non-MVE site, with the following differences.

When you take any of the following actions on one or more schedules, you are prompted for MVE validation if any schedule you have selected requires an MVE annotation or MVE electronic signature:

  • Add Exception(s)
  • Enable Schedule(s)
  • Disable Schedule(s)
  • Paste Weekly Schedule