Potential Problem Areas (PPA) widget for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The Potential Problem Areas widget for MVE on Metasys UI functions in the same manner as for a non-MVE site, with the following differences:

On MVE sites, the PPA widget displays only the points information, with no tabs. Fault information, with separate tabs for Points and Faults, is available on non-MVE sites.