Logic Viewer and Editor widget for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

The Logic Viewer and Editor widget for MVE on Metasys UI function in the same manner as for a non-MVE site, with the following differences.

When you use the Logic Editor in MVE on Metasys UI to modify a control system that requires an MVE annotation and/or MVE electronic signature, you are prompted for MVE validation when you save your changes.

On a non-MVE site, you can use the Logic Editor in the Metasys UI to add and delete child systems while you are editing a parent control system. For MVE sites, add and delete child systems directly in the Network tree within the Metasys UI. Alternatively, you can use the Logic Editor in JCT.
Note: After adding a child system through the Network tree, you must view, modify, and save its parent system before the child system starts executing any of its logic. This also ensures the parent's logic diagram shows the child system correctly.