Action Tables widget for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The Action Tables widget for MVE on Metasys UI functions in the same manner as for a non-MVE site with the following difference.

If you use the Action Tables widget to modify an interlock or multiple command object that requires an MVE annotation or MVE electronic signature, you are prompted for MVE validation when you save your changes.