User Menu for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

The User menu provides similar functionality on an MVE site as for an non-MVE site, with some differences.

The User menu provides access to any Metasys UI features that are available on an MVE site. Certain Metasys UI features, such as Graphics Manager, are available in Metasys UI for only non-MVE sites. See the various feature sections for details.

When you open the About window from the User menu for MVE on Metasys UI, you can view the license status for various Metasys features. On an MVE site, the MVE license includes SMP UI access without a separate SMP license. In this case, the SMP feature shows as Unlicensed in the About window but you are still able to log in to SMP UI for the MVE site.