Network Security for MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

Cyber Health Dashboard: The Cyber Health Dashboard for MVE on Metasys UI provides the same functionality on an MVE site as for an non-MVE site. Refer to Cyber Health Dashboard for details.

Device Pairing: Device Pairing does not require any MVE validation. The Device Pairing feature for MVE on Metasys UI provides the same functionality on an MVE site as for a non-MVE site. Refer to Device Pairing for more details.

BACnet/SC Management: For MVE on Metasys UI, you can use the BACnet/SC Management feature to view BACnet/SC certificate information for devices on the Metasys site. Use BACnet/SC Management in JCT to manage the certificates, including requesting new certificates, importing certificates, deleting unused signing certificates, and setting the BACnet IP communication mode for any engines.

You can also use MVE on Metasys UI to set the BACnet IP communication mode for an engine through its Network dashboard. Refer to the Network tab in the engine's Detail widget. A prompt appears for MVE validation when you change the IP communication mode for any validated engine that requires an MVE annotation or MVE electronic signature.