Log in to MVE on Metasys UI - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

The Log In page for Metasys UI provides similar functionality on an MVE site as it does for a non-MVE site with the following differences.

The Log In page for MVE on Metasys UI allows you to login using a local Metasys account or using an Active Directory service account with Active Directory/LDAP authentication. Login using your organizational account with ADFS authentication is available on only non-MVE sites. Refer to Accessing the Metasys UI for more details.
Note: Single Sign-on (SSO) and two-factor authentication (2FA) for Metasys UI logins are available on only non-MVE sites that are configured to use ADFS authentication.