The Advanced Search & Reporting feature on an MVE site has the same main tabs that are available on a non-MVE site: Search and Reports. For details see the sections below.
Search tab: The searching capability provided by the Search tab of the Advanced Search and Reporting feature is the same on an MVE site as for a non-MVE site. Refer to Advanced search, reporting, bulk commanding, and bulk modifying for more information.
If you open Commanding or use Bulk Command for one or more items in the search results on the Search tab, see Commanding for MVE on Metasys UI.
If you use Bulk Modify for one or more items in the search results on the Search tab, see Commanding for MVE on Metasys UI.
Reports tab: The Reports tab has the same secondary tabs that are available on a non-MVE site: Base and Saved From Search. The base reports available on the Base tab are the same on an MVE site as for a non-MVE site. The Saved From Search tab provides scheduled reports, that are supported only on non-MVE sites because actions on that tab that affect report templates and scheduled reports are not audited. For more details, refer to Reporting.