When you are adding item references to one of the site object’s Validated Environment attributes for including or excluding MVE electronic signatures or MVE annotations listed in Table 1, you can use both explicit and wildcarded item references.
Explicit item references: use an explicit item reference to include or exclude a particular object for MVE signatures and/or MVE annotations based on its fully qualified reference (FQR). An explicit item reference is one that exactly matches a specific object’s FQR. You provide an explicit item reference by typing or pasting an object’s full FQR into the edit field. See Table 1 for examples of explicit item references.
Wildcarded item references: use a wildcarded item reference to include or exclude a set of objects for MVE signatures and/or MVE annotations based on pattern matching for their FQRs. A wildcarded item reference is one that contains one or more asterisks (*) that will match any character(s) in the objects’ FQRs. You provide a wildcarded item reference by typing or pasting a wildcarded string into the edit field. See Table 1 for examples of wildcarded item references.
Modifying Validated Environment attributes
- Click or tap the value of the attribute. A separate edit window opens for the attribute similar to that shown in the figure below.
- Use the + symbol to add a new item reference row and then enter an explicit or wildcarded item reference in the edit field. Repeat to add additional item references.
- Use the delete symbol to remove a selected row from the list.
- Use the arrow symbols to move a selected row up or down.
- Click Save.
- If the site object is a validated object, the MVE Validation window opens. Provide the all required values and submit the MVE validation.
| Example | Reference type | Description |
|---|---|---|
| MAIN-ADX:MAIN-ADX/$site | Explicit | Site object only. |
| MAIN-ADX:MAIN-ADX | Explicit | ADX device object only. |
| MAIN-ADX:SNX-BLDG-3 | Explicit | Engine SNX-BLDG-3 only. |
| MAIN-ADX:SNX-BLDG-3/FC-1.AHU-02 | Explicit | Field device AHU-02 only (under the FC-1 MSTP trunk on engine SNX-BLDG-3). |
| MAIN-ADX:SNX-BLDG-3/FC-1.AHU-02.ZN-SP | Explicit | Field point ZN-SP only (on the AHU-02 field device under the FC-1 MSTP trunk FC-1 on engine SNX-BLDG-3). |
| * | Wildcarded | All objects on the site, including the site object and the ADX device object. |
| MAIN-ADX:SNX-BLDG-3/* | Wildcarded | All objects on engine SNX-BLDG-3 (but does not include the engine itself). |
| MAIN-ADX:SNX* | Wildcarded | All engines on the site that start with SNX as well as all objects on those engines. |
| MAIN-ADX:SNX-BLDG-3/FC-1.AHU-02* | Wildcarded | Field device AHU-02 (under the FC-1 MSTP trunk on engine SNX-BLDG-3) and all of its field points. |
| MAIN-ADX:SNX-BLDG-3/*ZN-SP | Wildcarded | All objects under engine SNX-BLDG-3 with an FQR that ends in ZN-SP. |
| *ZN-* | Wildcarded | All items on the site that have ZN- at any location in their FQR. |
| MAIN-ADX:MAIN-ADX/$FacilityGraphics.* | Wildcarded | All Metasys UI graphics on the ADX. |
| MAIN-ADX:MAIN-ADX/$FacilityTrendStudies.* | Wildcarded | All Metasys UI trend studies on the ADX. |