How do I configure a predefined MVE electronic signature reason? - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
To configure a predefined MVE electronic signature reason, complete the following steps.
  1. Open the User menu.
  2. Tap or click Administrative Tasks.
  3. Tap or click Site Settings.
  4. Tap or click Electronic Signatures.
  5. In the Predefined Electronic Signature Reasons section, tap or click the + symbol.
  6. Enter the text for the newly created predefined electronic signature reason. Select the check box and use the arrows to change the order of the predefined electronic signature reasons, if required.
  7. Tap or click SAVE.