What is an MVE site?
An MVE site consists of a validated MVE site director (ADX) plus one or more validated child engines. An MVE site can optionally include non-validated engines.
On an MVE site, the validated ADX site director and its validated engines are both types of validated devices.
What is a validated MVE site director?
- It is at the same Metasys release as its site director ADX.
- Its Is Validated attribute is set to True.
- Its engine model is supported as a validated device for MVE.
From Release 13.0, Metasys UI is provided on child engines as the primary user interface for directly logging on to the engine. When you use a supported web browser to access Metasys UI on to a validated child engine on an MVE site, the engine's audits and alarms are view-only. For details, see Alarms and audits for MVE on Metasys UI.
What are validated and non-validated objects?
When an object on a validated device requires an MVE annotation, MVE electronic signature, or both, the object is considered a validated object.
When an object on a validated device requires neither an MVE annotation nor an MVE electronic signature, the object is considered a non-validated object.
What are validated and non-validated audits?
When an audit is associated with a validated object, the audit is considered a validated audit. The object associated with an audit is identified by the audit's values for Item and Item Reference.
Any audit associated with a non-validated object is considered a non-validated audit.
Any audit associated with an object that does not exist as a Metasys object on the site is considered a non-validated audit. This includes audits associated with objects that have been deleted or removed from the site.
What are validated and non-validated alarms?
When an alarm is associated with a validated object, the alarm is considered a validated alarm if it meets the alarm priority thresholds for requiring an MVE annotation, an MVE electronic signature, or both. The object associated with an alarm is identified by the alarm's values for Item and Item Reference.
Any alarm associated with a non-validated object is considered a non-validated alarm.
Any alarm associated with an object that does not exist as a Metasys object on the site is considered a non-validated alarm. This includes alarms associated with objects that have been deleted or removed from the site.
An alarm that is associated with a validated object but meets neither the alarm priority threshold for requiring an MVE annotation nor the alarm priority threshold for requiring an MVE electronic signature is considered a non-validated alarm. See Setting alarm priority thresholds for requiring MVE electronic signatures and MVE annotations for information on configuring the alarm priority thresholds for requiring MVE annotations and MVE electronic signatures.
Licensing for MVE sites versus non-MVE sites
| Feature description | Feature | MVE sites | Non-MVE sites |
|---|---|---|---|
| Metasys Server | ADX | Required | Required |
| Metasys for Validated Environments | MVE | Required | Not supported1 |
| ADFS Authentication for Metasys | ADFS | Not supported | Optional |
| FIPS 140-2 for Metasys | FIPS-140 | Optional | Optional |
| Metasys BACnet Secure Connect | BACNET/SC | Optional | Optional |
| Metasys Fault Detection | FAULT | Not supported | Optional |
| Metasys Fault Triage | TRIAGE | Not supported | Optional |
| Monitoring and Commanding API | MONCMD-API | Not supported | Optional |
| Site Management Portal | SMP | Included with MVE | Optional |