Trend studies in Metasys UI on engines - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active

Trend Study Manager

The Trend Study Manager is available in Metasys UI only on servers. In Metasys UI on engines, you can create trend studies from the Network tree and use the Trend Study widget to view and edit the trend studies. Use SCT to add trend studies to user navigation views. For information about how to create, modify, and delete a trend study from the Network tree, see Trend studies in the Network tree.

How do I create a trend study on an engine?

To create trend studies on engines from the Network tree. For details, see How do I create a trend study in the Network tree?

How do I modify a trend study on an engine?

To modify a trend study on an engine, see How do I modify a trend study in the Network tree?

How do I delete a trend study on an engine?

To delete a trend study on an engine, see How do I delete a trend study in the Network tree?

Aggregated and raw data

Metasys UI on servers supports aggregated data. In Metasys UI on engines, only raw data is supported and displays by default when you open a trend study with trend extensions. There is no option available to select aggregated data. When you click the Information icon, the following message displays: Only raw data displayed.

To export raw trend data, complete the following steps:

  1. In the Network tree, select a trend study.
  2. In the Trend Study widget, click the Export icon.