What settings from the Metasys System Preferences are used in the Metasys UI?
The following table lists the settings from the Metasys System Preferences that are used in the Metasys UI. To access and change the settings in Metasys UI, open the User menu and go to and use Table 1 to change specific settings. For detailed instructions about editing the preferences, refer to Metasys UI Technical Bulletin (LIT-12012115) .
|
Metasys UI component |
Metasys System Preferences |
Where to change in Metasys UI |
|---|---|---|
|
Status Colors |
Status Colors |
|
|
New Alarm Indicator Available in: System Activity, Alarm Manager, Alarms list on smartphones |
New entry timeframe |
|
|
Alarm icons based on alarm priority Available in: System Activity, Equipment Activity widget, Alarms list, Alarm Manager, and Alarm Monitor |
Color |
|
|
Alarm Sound Available in: System Activity, Alarm Manager, and Alarm Monitor |
Alarm Sound Interval Audio File |
|
|
Audible Alarm Note: To get alarm sounds, you must first enable
audible alarms.
|
Enable Audible Alarm |
|
|
Trend Chart Line Color and Line Marker |
Line Color Line Marker |
|
|
Session Inactivity Never Terminate Note: To set the session inactivity or Never Terminate
setting, you must configure this setting for every user.
|
Terminate in (minutes) |
. Select the user and click on the Edit User icon in the Actions column. Open the Account Settings tab and navigate to the Inactive Sessions section.
|
What do the colors used in the Metasys UI mean?
The color preferences in the Metasys UI indicate the status of points, such as Offline, Normal, and Alarm, for example. Color preferences are used throughout the Metasys UI, including the Alarm list on phone platforms. To view the default color preferences in the Metasys UI, open the User menu and go to .
How do I change the color preferences?
You can change the color preferences in Metasys UI. Open the User menu and go to .
How long does it take for changes to the color preferences to update?
Changes made to the color preferences can take up to five minutes to update in the Metasys UI.