What are annotations?
When do I use annotations?
- an operational task that should be performed in response to a cause or condition that prompted a user change or an alarm event
- a reason for an adjust, operator override, or release command
Unless the Administrator enforces annotations at a site level, the following annotations are optional.
- Annotations added to a user change: You can enter annotations when you command from the Command window or when you bulk command from the Bulk Command window. You can also add an annotation to the user change entry for the command in the Equipment Activity widget.
- Annotations added to a system change: You can add annotations to the system change entry in the Equipment Activity widget.
- Annotations added to an alarm instance: You can add annotations to the alarm instance in the Alarm Manager, in Alarms on your smartphone, or to the alarm entry in Equipment Activity widget. Additionally, discards and acknowledgments of an alarm appear as annotations.
- Annotations added when discarding an audit in System Activity.
Can I edit or delete existing annotations?
You cannot edit or delete existing annotations. Instead, add a new annotation to the user change, system change, or alarm instance.
Where can I view and add annotations?
- Alarms in the Equipment Activity widget, the Alarm Manager, and the Alarms (only available on phone platforms)
- System changes or user changes in the Equipment Activity widget
- Audits in System Activity
- In the Command window when you command an object
- In the Bulk Command window when you bulk command objects
- In the Single Discard window when you discard an audit or alarm
- In the Bulk Discard window when you discard multiple audits or alarms
- In the Single Acknowledge window when you acknowledge an alarm
- In the Bulk Acknowledge window when you acknowledge multiple alarms
What do the icons used for annotations represent?
The following table describes the icons that you see in connection with annotations.
Icon | Icon name | Feature | Description |
---|---|---|---|
|
Annotations | Equipment Activity widget, System Activity | Annotations are available to view. |
|
Annotations | Alarm Manager and Alarms (phone), System Activity | Annotations are available to view. |
|
Add Annotation | Equipment Activity widget, Alarm Manager, and Alarms (phone), System Activity | Add an annotation. |
How do I view annotations in the Equipment Activity widget?
- Navigate to the Equipment Activity widget.
- Tap or click on a user change, alarm instance, or system change. When a user change, alarm instance, or system change has annotations to view, the annotations icon appears below the short name of the point.
- Tap or click View/Add Annotation.
How do I view annotations in the Alarm Manager (computer or tablet) or in Alarms (phone)?
- Navigate to the Alarm Manager (computer or tablet) or Alarms (phone).
- Tap or click on an alarm. The alarm details open. When an alarm occurrence has annotations to view, the annotations icon appears.
- Tap or click the annotations icon.
Note: Annotations added to an alarm do not appear in the annotations for a new occurrence of an alarm. To view annotations for a particular occurrence, tap or click the annotations icon next to the occurrence.
How do I add an annotation in the Equipment Activity widget?
- Navigate to the Equipment Activity widget.
- Tap or click on a user change, alarm instance, or system change.
- Tap or click View/Add Annotation.
- Tap or click the Add Annotation icon. The Annotations window opens.
- You can select a predefined annotation from the drop-down,
or you can enter your own annotation in the text box. Note: You can select a predefined annotation, then change the predefined text manually in the text box. This change is not subsequently reflected in the drop-down in Metasys UI or in SMP. The changed text only applies to that particular action. You can configure the predefined annotations in Metasys UI. See How do I configure a predefined annotation? for more information.
- Tap or click ADD. Your annotation appears in the Annotations window.
How do I add an annotation in the Alarm Manager (computer or tablet) or in Alarms (phone)?
- Navigate to the Alarm Manager (computer or tablet) or to Alarms (phone).
- Tap or click on an alarm.
- Tap or click
Annotations. Note: Annotations added to an alarm do not appear in the annotations for a new occurrence of an alarm. To add annotations for a particular occurrence, tap or click Annotations next to the occurrence.
- Tap or click the Add Annotation icon. The Annotations window opens.
- You can select a predefined annotation from the drop-down,
or you can enter your own annotation in the text box. Note: You can select a predefined annotation, then change the predefined text manually in the text box. This change is not subsequently reflected in the drop-down in Metasys UI or in SMP. The changed text only applies to that particular action. You can configure the predefined annotations in Metasys UI. See How do I configure a predefined annotation? for more information.
- Tap or click ADD. Your annotation appears in the Annotations window.
How do I add an annotation in the Command window?
- Tap or click the point's value to open the Command window.
- Select the command type from the
Command drop-down menu. Note: On tablets and phones, tap the Command field to select the command type from the list and tap Done.
- Command the point as desired.
- You can select a predefined annotation from the drop-down,
or you can enter your own annotation in the text box. Note: You can select a predefined annotation, then change the predefined text manually in the text box. This change is not subsequently reflected in the drop-down in Metasys UI or in SMP. The changed text only applies to that particular action. You can configure the predefined annotations in Metasys UI. See How do I configure a predefined annotation? for more information.
- Tap or click in the Add Annotation field to enter an optional annotation.
- Tap or click SAVE.
- When adding annotations while commanding points that have audits forwarding from engines to the Site Director, the annotations may not appear immediately in the Equipment Activity widget.
- Any Samsung™ phone for Android performs best when you use a third-party keyboard for commanding. You first need to download a third-party keyboard. To use a third-party keyboard, go to and select a third-party keyboard. The location for changing the keyboard may vary depending on your device.
How do I add an annotation in the Bulk Command window?
- After you have selected your objects, select a command from the drop-down menu.
- You can select a predefined annotation from the drop-down,
or you can enter your own annotation in the text box. Note: You can select a predefined annotation, then change the predefined text manually in the text box. This change is not subsequently reflected in the drop-down in Metasys UI or in SMP. The changed text only applies to that particular action. You can configure the predefined annotations in Metasys UI. See How do I configure a predefined annotation? for more information.
- Tap or click NEXT to see a preview of your selected command.
How do I add an annotation in System Activity?
- Select a single audit or multiple audits by tapping or clicking the check box next to the audits.
- Tap or click ACTIONS in the upper left of the screen.
- Select Annotate. The Single Annotate window opens when you select one audit. The Bulk Annotate window opens when you select multiple audits.
- Select a predefined annotation or enter your own comment in the text box.
- Tap or click ADD.Note: After a bulk action on a large number of items in System Activity, you may experience one or more of the following:
- A delay in annotation icon updates
- A delay in activity icon status updates
- The Metasys UI becomes unresponsive for a time
- The System Activity feature does not properly display after selecting a new tab
If you experience any of the issues listed above, wait for 10 to 20 seconds after any bulk operation such as bulk annotation, acknowledge, or discard. If the issues do not resolve after a short time, refresh your browser.
- Tap or click on an audit. The audit details flyout pane opens.
- Tap or click the Annotations hyperlink. The Annotations window opens.
- Tap or click the Add Annotation icon in the Annotations window.
- Select a predefined annotation or enter your own comment in the text box.
- Tap or click ADD.
How do I configure a predefined annotation?
- Open the User menu.
- Tap or click Administrative Tasks.
- Tap or click Site Settings.
- Tap or click Annotations.
- In the Predefined Annotations section, tap or click the + symbol.
- Enter the text for the newly created predefined annotation. Select the check box and use the arrows to change the order of the predefined annotations, if required.
- Tap or click SAVE.
Why can I not add an annotation?
To add annotations to an alarm, you must have the Manage Item Event Permission. To add annotations to an audit, you must have the View Metasys Status and Manage Audit History system access privileges. See What permissions and privileges do I need to add annotations? for more information.
If an alarm or an audit is discarded, you can no longer add annotations to the alarm or to the audit.
What permissions and privileges do I need to add annotations?
Type of annotation |
Required permissions or privileges |
---|---|
Adding annotations to an alarm |
Manage Item Event permission |
Adding annotations to a system change |
Manage Audit History system access privilege |
Adding annotations to a command in the Equipment Activity widget (user change) |
Manage Audit History system access privilege |
Adding annotations in the Command window of a point |
Appropriate permissions to command the point and Manage Audit History system access privilege |
Adding annotations to an audit in System Activity |
View Metasys Status and Manage Audit History system access privileges |
Are the annotations created in the Metasys UI available to view in the Site Management Portal (SMP)?
Yes. Use the Event Viewer in SMP to look at alarm event message's annotations created in the Metasys UI. Use the Audit Viewer in SMP to look at the system change's annotations or user change's annotations created in the Metasys UI.
Can I export or print annotations?
You can export annotations that appear in the Annotations window on a computer. The export function is not supported on tablets or phones.
To export annotations that appear in the Annotations window, click the export icon. You can export annotations to a .csv file and open the file in any supported spreadsheet software.
- the user name of the user that entered the annotation
- the timestamp of the annotation
- the annotation text
To print the exported annotations, click the export icon to export the data to a .csv file. You can then print the .csv file.