Audible alarm feature (Alarm sounds) - Metasys - LIT-12011953 - Server - Metasys UI - 7.0.50

Metasys UI Help

Brand
Metasys
Product name
Metasys UI
Document type
User Guide
Document number
LIT-12011953
Version
7.0.50
Revision date
2024-03-19
Product status
Active
Language
English

The audible alarm feature in Metasys UI is available to any logged-in user who has the feature enabled in their user profile. Refer to How do I enable or disable the audible alarm feature? for more information.

The audible alarm feature provides sounds to notify you when a new alarm that requires acknowledgement occurs. The sound that plays corresponds to the highest priority unacknowledged alarm that you have permission to view. If multiple alarms occur for different priorities, the sound for the highest priority alarm plays. Refer to When do alarm sounds play? for more information.

Administrators use Site Settings to configure the sound that plays for each alarm based on its alarm priority. Refer to How do I configure the alarm sounds? How do I use custom files for the alarm sounds? for more information.