Metasys upgrade software - Metasys - LIT-12011703 - Software Application - Metasys System - 13.0.50

Metasys System Software Purchase Options Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-12011703
Version
13.0.50
Revision date
2024-01-23
Product status
Active

Upgrade software is current-release Metasys software for upgrading products, such as the ADS/ADX, OAS, MVE, NAE85, and LCS85, at sites that have a previous major release of the Metasys software already installed . For example, upgrading Release 12.x or earlier software to Release 13.0. Metasys upgrade software packages are identified by a -6 suffix on the product code number.

Metasys upgrade software packages may also include upgrades to the current supported Microsoft SQL Server software. For example, upgrading an existing ADX10 to an ADX10SQL.

For major upgrades, such as upgrading Release 12.x or earlier to Release 13.0, you must purchase a current Metasys upgrade software package. You can upgrade from any previous major release to the current major release.

For minor upgrades, such as upgrading Release 10.0 to Release 10.1, your Johnson Controls representative can upgrade the site.

Note: Typically, there is no cost for Metasys software for minor upgrades. However, not all minor release software packages are at no cost. For more information, contact your local Johnson Controls representative.

To determine if you must re-license your upgrade software, see Licensing information.