Migration software is current Metasys software packages for upgrading an existing ADS or ADX to the current release version and migrating the ADS or ADX to a different number of users. For examples, see the following table. Metasys migration software packages are identified by a -8 suffix on the product code number. For software migration code number examples, see Table 3.
From Release 12.x or earlier |
To Release 13.x |
---|---|
5-User ADS | 10-User ADX |
25-User ADX | |
50-User ADX | |
100-User ADX | |
10-User ADX | 5-User ADS |
25-User ADX | |
50-User ADX | |
100-User ADX | |
25-User ADX | 5-User ADS |
10-User ADX | |
50-User ADX | |
100-User ADX | |
50-User ADX | 5-User ADS |
10-User ADX | |
25-User ADX | |
100-User ADX |
All software migrations require re-licensing after the migration. The software license reflects the number of users and the object count for which the software is licensed. For more information on licensing, see Licensing information.
The following table lists the history of Metasys servers and various tools with their release dates and release numbers, from year 2013 to the present.
Release date | Metasys Server1 , 2 | Metasys UI 3 | Metasys Launcher | SCT/SCT Pro/JCT 4 | NAE Update Tool | CCT |
---|---|---|---|---|---|---|
January 2013 | 6.0 | N/A | 1.1 | 6.0 | 6.0 | 10.0 |
June 2013 | 6.1 | N/A | 1.1 | 6.1 | 6.1 | 10.0 |
February 2014 | 6.5 | N/A | 1.2 | 6.5 | 6.5 | 10.0 |
July 2015 | 7.0 | 1.5 or 1.5.1 | 1.3 |
7.0 |
7.0 | 10.1 |
December 2015 | 7.0 | 1.5 or 1.5.1 | 1.4 | 10.0 | 10.0 | 10.1 |
September 2016 | 8.0 | 2.0 | 1.5 | 11.0 | 11.0 | 10.2 |
February 2017 | 8.1 | 2.1 | 1.6 | 11.1 | 11.1 | 10.2 |
August 2017 | 9.0 | 3.0 | 1.6 | 12.0 | 12.0 | 10.3 |
December 2018 | 10.0 | 4.0 | 1.7 | 13.0 | 13.0 | 13.0 |
September 2019 |
10.1 |
4.1 |
1.7 |
13.2 |
13.2 |
13.1 |
October 2020 | 11.0 | 5.0 | 2.0 | 14.0 5 | The NAE Update Tool continues to be a component of the SCT install. However, we encourage you to use SCT Pro instead of the NAE Update Tool. | 14.0 |
November 2020 | N/A | N/A | N/A | 14.1 | N/A | |
May 2021 | N/A | N/A | N/A | 13.3 and 14.2 | N/A | |
May 2022 | 12.0 | 6.0 | 2.0 | 15.0 | 15.0 | |
May 2023 | 12.0.50 | 6.0.50 | 2.0 | 15.0.4 | 15.0 | |
September 2023 | 13.0 | 7.0 | 2.0 | 16.0 | 16.0 | |
January 2024 | 13.0.50 | 7.0.50 | 2.0 | 16.0 | 16.0 |