Configuration tool use - Metasys - LIT-12011703 - Software Application - Metasys System - 13.0.50

Metasys System Software Purchase Options Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-12011703
Version
13.0.50
Revision date
2024-01-23
Product status
Active

You must license the Metasys Configuration Tools before use. These tools include the following:

  • System Configuration Tool (SCT), includes Johnson Controls System Configuration Tool (JCT)
  • Metasys Field Controller Package
  • Metasys Device Package
  • Controller Configuration Tool (CCT)
    • Johnson Controls Sensor/Actuator (SA) Bus Device Package
      Note: Johnson Controls Sensor/Actuator (SA) Bus Device Package is a licensed feature within the CCT product. You can access and download the content associated with this license separately through the Johnson Controls SA Bus Device Packages product on the License Portal. To ensure that the license applies to both CCT and the Johnson Controls SA Bus Device Packages product, import Johnson Controls SA Bus Device Packages before you license CCT.

For licensing information, refer to Software Manager Help (LIT-12012389) and the specific product installation guides for these tools.