Metasys for Validated Environments (MVE) - Metasys - LIT-1201526 - General System Information - Metasys System - 14.0

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
14.0
Revision date
2024-09-17
Product status
Active
Note: MVE is not supported at Release 14.0.
Metasys for Validated Environments (MVE) on Metasys UI is the newest offering from Johnson Controls for facilities that require regulatory compliance for the Building Management Systems (BAS). MVE controls environmental conditions and audits user management for critical environments, such as hospitals, research facilities, food production centers, and other production environments where tight control is crucial to product success.

MVE provides traceable electronic records, signatures, and time-stamped audit trails for facilities, helping customers comply with:

  • Food and Drug Administration (FDA) Title 21, Code of Federal Regulations Part 11
  • EU Annex 11 of the European Union Good Manufacturing Practice (EU GMP) regulations (European Medicines Agency [EMA] 2011)
  • Agency regulations around the world that deal with electronic records and electronic signature requirements
The MVE feature operates on an ADX and communicates to validated Network Engine models.
Important: At Metasys Release 13.0.50, the ADX and MVE software must be at 13.0.50 and the validated engines at 13.0.1.
Note: From Release 12.0.50, MVE capabilities are supported in Metasys UI, in addition to SMP. MVE also supports BACnet/IP or BACnet/SC devices.
Note: You need to purchase an add-on license to use MVE on the ADX Server and you can use either Metasys UI or SMP for MVE.