Enable the Warning Banner feature to display a selected warning before you log on to Metasys UI or access the Metasys Alarm Monitor.
The Warning Banner is a logon feature that displays as a text window. The information in the window is customized for the United States government agency where the Metasys system is installed. A warning banner contains information critical to any Metasys local or external user that attempts to access the Metasys UI from a Metasys system installed at an associated United States government agency. You must click OK or I AGREE to consent to the statement before you can access the Metasys UI log on window or the Metasys Alarm Monitor.
Warning banners are supported on the following servers and engines running Metasys UI that are configured as Site Directors: ADS, ADX, OAS, NAE85, LCS85, and network engines.