Metasys UI - Metasys - LIT-1201526 - General System Information - Metasys System - 14.0

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
14.0
Revision date
2024-09-17
Product status
Active

The Metasys UI is an HTML5-compliant web interface that provides device-agnostic access to Metasys from smartphones, tablets, and computers. The Metasys UI is an intuitive interface that reduces learning time, maximizes productivity of operators, and provides a seamless user experience no matter what type of client device is used to access the system. The client device does not require any additional software installation—no Java™, Microsoft Silverlight®, Adobe®, Flash® or any other software from an online app store.

The Metasys UI is included with SNE, SNC, NAE85, LCS85 series network engines, and any Metasys server: ADS, unified and split ADX, OAS, and ADS-Lite. You must license the server software to log on to the Metasys UI.

For more information about Metasys UI, refer to the Metasys UI Help (LIT-12011953) and the Metasys UI Technical Bulletin (LIT-12012115) .